Technical FAQs

Ask a Question

Is there a door operated mechanism for Powerpact D frame breakers.

Yes, customer will need to order in components, Operating mechanism is 9421LD7, 9421LS13 is the long handle with support bracket, 9421LS8 is the short handle which does not require a support bracket, and the 9421LH6 painted metal handle. For the Chrome handle use 9421LC46.

CTA-ID : 2052276
Was this helpful?
What can we do to improve the information ?