Technical FAQs

Ask a Question

What type 1 surge protection device is available for 600V or 480V single phase service ahead of a main circuit breaker in a panel?

Square D/Schneider Electric has no single phase surge protection product in 600V or 480V voltage range at this time.

CTA-ID : 2052838
Was this helpful?
What can we do to improve the information ?