Technical FAQs

Ask a Question

What is the Joules rating on a catalog number TVS120XR40B?

The TVS120XR40B is rated at 40KA per phase. There is no Joules rating used on industrial surge protection, since Joules rating is not recognized by ANSI.


CTA-ID : 2052129
Was this helpful?
What can we do to improve the information ?