Technical FAQs

Ask a Question

What are the clearance requirements around the surfaces of Ventilated Transformers.

Issue:
Vent openings on Ventilated Transformers require clearance from obstructions
 
Product Line:
LV Transformers
 
Environment:
Applies to all Ventilated Transformers from SquareD/Schneider Electric
 
Cause:
Energized Ventilated Transformers generate heat which must be carried away by airflow out of the vents on front and back of the enclosure
 
Resolution:
Clearances front/rear, sides and top:
The ventilation openings on EE type Ventilated Transformers must have a minimum of 3" clearance from vertical surfaces such as walls, bulkheads and other equipment.   The sides and back surfaces of EX type Ventilated Transformers must have a minimum of .5" from vertical surfaces such as walls, bulkheads and other equipment.
Non-flammable, non-heat-sensitive equipment can be placed directly in contact with the right and left sides.
It is not recommended to place heat sensitive equipment above the transformer and nothing should contact the top cover.
If one transformer is going to be placed above another, a minimum of 3' ( 36" ) should be maintained from the top surface of the lower transformer and the bottom surface of the upper transformer. 



CTA-ID : 2052857
Was this helpful?
What can we do to improve the information ?