Technical FAQs

Ask a Question

Is a Class 30 trip available on the Motor Logic Overload Relays?<br />

Product Line:
 
NEMA style Overload Relays

Resolution:
 No, only Class 10 or Class 20 trip is available.


CTA-ID : 2052819
Was this helpful?
What can we do to improve the information ?