Technical FAQs

Ask a Question

What is provided in the QOCGK2 or QOCGK2C Generator Interlock Kit?

Product features

Product Line:
QO load centers

Generator interlock kit


The kit includes a sliding mechanism that interlocks the QOM2 Main Breaker with a branch mounted, back-fed QO breaker. It will also include the retaining mechanism for the branch mounted, back-fed QO breaker. Installation Instructions, mounting template and labeling are also included.

NOTE: When stock is depleted on the QOCGK2, order QOCGK2C. The only difference is the packaging material.

CTA-ID : 2052760
Was this helpful?
What can we do to improve the information ?