Technical FAQs

Ask a Question

How are the standard lugs removed from the MJ or MG breaker?

Turn the breaker over so that the back is accessible. Then pry open the cover that prevents access to the lug hardware and unscrew the lug cap screws.

CTA-ID : 2052142
Was this helpful?
What can we do to improve the information ?