Technical FAQs

Ask a Question

What is the S5812 on a FAL26030S5812 breaker?

The (S) was used to indicate a special, which we no longer use. The 5812 was for factory installed rear-connected studs, which we no longer offer as factory installed. Customer should purchase a FAL26030 breaker with (2) FAS20 and (2) FAS42 studs.


CTA-ID : 2052856
Was this helpful?
What can we do to improve the information ?