Technical FAQs

Ask a Question

What do the numbers designate in an FAL circuit breaker part number?

The first number represents the number of poles, the second number represents the voltage rating and the last 3 numbers designate the amperage. For example: FAL32040 is 3 poles, 240V, and 40 amps. FAL14100 is single pole, 480V, and 100 amps, and an FAL26100 is 2 poles, 600V, and 100 amps, etc.

CTA-ID : 2052983
Was this helpful?
What can we do to improve the information ?