Technical FAQs

Ask a Question

Can a pulsation plug be field installed on an 9013FSG2?

Yes. The pulsation plug fits into the internal pressure connection between the pipe threads in to the same point on the switch capturing the pulsation plug.

CTA-ID : 2052981
Was this helpful?
What can we do to improve the information ?