Technical FAQs

Ask a Question

REVISION TO FAQ 2003242: CHANGED PART # 51568 TO CURRENT PART # 515608 <br /><br />What is the catalog number and description for a hookstick for busway plug-in devices?

The hooksticks are made of fiberglass and come in two sizes. Part number 515608 is 8 feet long and 515614 is 14 feet long.


CTA-ID : 2052960
Was this helpful?
What can we do to improve the information ?