Technical FAQs

Ask a Question

Do the EZM tap boxes such as EZM1400TB have mechanical lugs or compression type lugs on the incoming terminals?

Mechanical lugs are standard on EZM main section tap boxes, circuit breakers and fusible switches. Compression lugs are an option on some units, but are never standard.


CTA-ID : 2052930
Was this helpful?
What can we do to improve the information ?