Technical FAQs

Ask a Question

Where on the EZM devices is the Short Circuit Series Ratings (SCCR) label located. <br />

The Short Circuit Series Ratings (SCCR) on the EZM devices are located in the branch devices. The 3-Tier ratings are located in the downstream load centers.



CTA-ID : 2052110
Was this helpful?
What can we do to improve the information ?