Technical FAQs

Ask a Question

Is it possible to make a 480v, 50hp 2speed, single winding, constant hp bucket 54`` high? The standard 60``<br />

The 50HP 2S1W constant HP unit requires Nema Size 4 starters which take up 60``. There is no way to reduce this size to 54``.
We can supply a 50HP 2S1W CVT unit in 51`` (uses Nema Siz 3 starter).


CTA-ID : 2051925
Was this helpful?
What can we do to improve the information ?