Technical FAQs

Ask a Question

Is it possible to monitor phase loss output with a Power Pact trip unit, such as used on a PowerPact RJ2000 breaker? Is the trip unit able to output a signal that simulates the dry contact output of a phase failure relay? Can it trigger a shunt trip installed in the breaker?

These circuit breaker trip units do not have dry output contacts that work similarly to a phase failure relay. The application would have to use a separate phase failure relay and installed shunt trip in the breaker.

CTA-ID : 2052755
Was this helpful?
What can we do to improve the information ?