Technical FAQs

Ask a Question

How do you enter through the back splice in MCC`s?

For through the back splice, decide which sections will be connected through the back. Make sure that they are entered in single shipping splits. delivery code `F` for tin plated copper bussing. All other bussing types are `H` delivery. You are limited to 1200A horizontal bussing. Neutral bus is not available in through the back application. It can be done in 15 or 20`` deep application.

CTA-ID : 2052063
Was this helpful?
What can we do to improve the information ?