Technical FAQs

Ask a Question

Can the interior assembly from QO330L200GRB be installed in a QO318L200GRB since they use the same size box, 6R?

Issue:
Product Design features

Product Line:
QO load centers

Environment
Interior bussing

Cause:
Application or maintenance

Resolution:
No. The labeling on wiring diagram would be incorrect and UL Listing is voided.


CTA-ID : 2051944
Was this helpful?
What can we do to improve the information ?