Technical FAQs

Ask a Question

Do the Powerpact D frame breakers have finger safe covers?<br />

Yes, the part number for the Finger Safe Covers for the Powerpact D frame breaker is 36965. These can only be used with the power distribution connectors.


CTA-ID : 2051992
Was this helpful?
What can we do to improve the information ?