Technical FAQs

Ask a Question

Customer has a HOM4060M200C loadcenter. What is the neutral terminal kit, LK100AN is used for?

This is a neutral lug kit, included with the load center that is installed on the neutral bar for a larger neutral conductor if required.

CTA-ID : 2051945
Was this helpful?
What can we do to improve the information ?