Technical FAQs

Ask a Question

What is the Bus rating of the catalog number SC2040M200F, Series M02?

Product design features

Product Line:
Combination Service Entrance Devices

Bus rating


The bus rating for the Series M02 ONLY, is 225Amp Max. and the Mains rating is equal to the ampacity of the installed Main Breaker, which is 200A Max. The wiring diagram will indicate that a Main Breaker can ONLY be used up to 200A maximum.

NOTE: The SC2040M200F Series M02 will be Obsolete once stock is depleted and replaced by the SC2040M200PF Series M01.

CTA-ID : 2052800
Was this helpful?
What can we do to improve the information ?