Technical FAQs

Ask a Question

What is the short circuit current rating for a D324NRB General Duty Safety Switch?

The short circuit current rating is 10k AIC when used with standard H or K type fuses and 100k AIC when used with a Class R (with HRK1020 kit installed) or J fuses.


CTA-ID : 2052696
Was this helpful?
What can we do to improve the information ?