Technical FAQs

Ask a Question

What is the part number for the sub-pan used to install a QB, QD, QG or QJ sub-feed circuit breaker in an NQOD panel with factory installed provisions (space only) for a sub-feed breaker?<br />

The mounting holes in the sub-feed breaker mounting pan are for a KA breaker. If a QB, QD, QG or QJ sub-feed breaker is required instead, an additional sub-pan is needed. Qty (1) sub-pan is used to mount qty (1) QB, QD, QG or QJ type subfeed breaker. For a 400 or 600A main breaker NQOD panelboard, the part number for the sub-pan is 80110-054-02. For a 400 or 600A main lugs only panelboard, the  part no. 80110-652-01 is now obsolete with no replacement .Quantity  (4) mounting screws, part no. 21590-170-81, are also needed.


CTA-ID : 2052002
Was this helpful?
What can we do to improve the information ?