Technical FAQs

Ask a Question

What size power fuse clips are used on a size 1 starter unit at 480V?<br />

30A fuse clips. Class R fuse clips require qty. (3) 40555-122-50 and qty. (1) 80409-424-50.
Class J fuse clips require qty. (3) 40555-122-50 and qty. (1) 40555-125-50
Class H fuse clips require qty. (3) 40555-122-50 and qty. (1) 40555-125-50


CTA-ID : 2052030
Was this helpful?
What can we do to improve the information ?