Technical FAQs

Ask a Question

What are the repair parts for the HU361SS, series F6? (may be shown as F06)

The repair parts for the HU361SS, series F6 (F06) are as follows. No other parts are available.

-Line Base Assembly - 4056642650 (arc suppressor not included)
-Line Base mounting screw - 4020516001 (3 required)
-Arc Suppressor Assembly - 4056669451
-Arc Suppressor mounting screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lugs)
-Lug Keps Nuts - 4020515401
-Mechanism Assembly - 4056610750 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056808050 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056808101 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screw - 2194900001 (2 required)
-Ground Lug - 4025101652 - (2 total required)
-Ground Lug Mounting Screw ﾿ 4020513503



CTA-ID : 2052948
Was this helpful?
What can we do to improve the information ?