Technical FAQs

Ask a Question

Will the H364NRB accept a 3`` hub, B300?

The standard hub opening provided in the top endwall will accept at B type hub, up to 2.5`` maximum. A field cut hole will be required to use a larger hub than 2.5``.


CTA-ID : 2052237
Was this helpful?
What can we do to improve the information ?