Technical FAQs

Ask a Question

What is the catalog number for the Control Wire Tap Lug for an MH or MHL breaker?

AL900MAT is one lug that accepts (3)#3/0 AWG to 500 kcmil.
AL1000MAT is one lug that accepts (4)#1/0 AWG to 350 kcmil.


CTA-ID : 2052459
Was this helpful?
What can we do to improve the information ?