Technical FAQs

Ask a Question

What are the recommended HVL/cc storage temperatues?

Close to room temperature 20-25 C (68-77 F). The goal is to have the least amount of humidity possible. Typically 100 Watts per section. 200 Watts if very humid environment.

CTA-ID : 2052390
Was this helpful?
What can we do to improve the information ?