Technical FAQs

Ask a Question

What is the maximum AC mains wire distance allowable to connect an SDSB1175C surge suppressor to a panelboard or load center?

Issue:
What is the maximum AC mains wire distance allowable to connect an SDSB1175C surge suppressor to a panelboard or load center?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The wire length should be very short, about 18 inches from the panel bussing, maximum. Longer lengths drastically reduce the effectiveness of the Surge Suppression of the SDSB1175C.


CTA-ID : 2051995
Was this helpful?
What can we do to improve the information ?