Technical FAQs

Ask a Question

What is the SCCR (Short Circuit Current Rating) of a QO Main Breaker Load Center?

Issue:
Application

Product Line:
QO Load Center

Cause:
Application and selection

Resolution:
QO Single Phase Main Breaker Load Centers supplied with a QOM1-VH (125A max) or QOM2-VH (225A max) main breaker are rated 22,000 AIC Maximum.
QO Three Phase Main Breaker Load Centers supplied with a QDL main breaker are rated 25,000 AIC Maximum. The factory installed QDL main breaker can be replaced with a QGL 65,000 AIC or QJL 100,000 AIC Main Breaker.


CTA-ID : 2051965
Was this helpful?
What can we do to improve the information ?