Technical FAQs

Ask a Question

Will the PQ3620G work with the vertical mounting kit?<br /><br />

No. Use PS3620G for vertical riser applications only. Vertical mounting kit is used with 400A and 600A PBQ units.



CTA-ID : 2052023
Was this helpful?
What can we do to improve the information ?