Technical FAQs

Ask a Question

Can SquareD/Schneider Electric supply Transformers with Stainless steel enclosures with an unpainted finish?

Stainless Steel Enclosures

Product Line:
LV Transformers

Applies to Low Voltage Transformers by SquareD/Schneider Electric

Requirement for Transformers with Stainless Steel Enclosures


This can be done,  but the Transformer will have weld marks, a machine stripe on the steel to ID as 316 SS, etc.  It is a mill finished dull stainless steel, not a polished or matte silver home appliance type finish. The local SquareD/Schneider Electric Field Office will provide special p/n and pricing.

CTA-ID : 2052201
Was this helpful?
What can we do to improve the information ?