Technical FAQs

Ask a Question

What are the restrictions for a 5/15kV HVL switch on the primary of a Type 36 Substation?

Restrictions are: Single main transformer switch only, Front access only, 750KVA maximum dry type transformer, Current limiting fuses only, Two cables per phase maximum, Distribution class surge arresters only, No instrument transformers or metering, 12`` minimum top pullbox required for top or bottom cable entry.


CTA-ID : 2052391
Was this helpful?
What can we do to improve the information ?