Technical FAQs

Ask a Question

Does Schneider Electric / Square D offer a shunt trip mechanism on QMB or QMJ fusible switches?

Issue:
Product features

Product Line:
QMB/QMJ

Cause:
Clarification of product features

Resolution:
QMB and QMJ fusible switches are strictly a mechanically operated device. A electrically operated shunt trip mechanism is not available for the QMB or QMJ fusible switches. For a shunt trip application, consider using a QMB circuit breaker unit with a field installed shunt trip accessory or consider using an I-Line circuit breaker panel board instead of the QMB fusible switch panel board.


CTA-ID : 2052360
Was this helpful?
What can we do to improve the information ?