Technical FAQs

Ask a Question

What does the ``e`` on a 1S67Fmean ?

The ``e`` on a 1S67F is meant to indicate a foot note that was left out of the Digest. It indicates that the 1 KVA transformer was IEC rated only at 750VA, not the full 1 KVA (1000 VA). This is true only on the 1 KVA version.
This only affects IEC tested rating, it is a full 1 KVA transformer when used domestically


CTA-ID : 2052898
Was this helpful?
What can we do to improve the information ?