Technical FAQs

Ask a Question

What is the meaning of the (T) in the catalog number for some types of open style starters, such as # 8536SCTO3V02S?

The ``T`` embedded in the part number indicates addition of auxiliary terminals on the line side of the overload block of Size 0 through 2. Size 3 and above are already configured and do not require these auxiliary terminals


CTA-ID : 2052329
Was this helpful?
What can we do to improve the information ?