Technical FAQs

Ask a Question

What is the part number for the reset for a Size 3 starter with melting alloy overloads?<br />

80420-302-53
This is also the same for size 4 starter with melting alloy overloads.


CTA-ID : 2052050
Was this helpful?
What can we do to improve the information ?