Technical FAQs

Ask a Question

Is the 82345 double throw safety switch 100% rated?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Endurance testing

Cause:
Application

Resolution:
Yes, since this is a Non-Fusible Switch, it is rated at 100% of its nameplate rating of 400Amps, current rating.


CTA-ID : 2051031
Was this helpful?
What can we do to improve the information ?