Technical FAQs

Ask a Question

Are any low current level or hermetically sealed 9999SX auxiliary contacts available for PLC and signalling applications?

No. There are no low level or hermetically sealed 9999SX type contacts currently available. However the design of the contacts makes them suitable for most applications except very low signal levels and bad (corrosive) environments.


CTA-ID : 2051296
Was this helpful?
What can we do to improve the information ?