Technical FAQs

Ask a Question

How many magnetizing current interruptions can the 15kV 600A HVL switch do?

80 at 9.5 to 62.8 amps.
20 cycles at each level
9.5 Amps at 12.5% PF
18.8 Amps at 10% PF
31 Amps at 12% PF
45 Amps at 10% PF
62.8 Amps at 13.2% PF


CTA-ID : 2050973
Was this helpful?
What can we do to improve the information ?