Technical FAQs

Ask a Question

Can a 40amp tenant breaker be used in a EZM114225 that uses the Q-Frame breakers?

Yes, need to use an adapter EZM125QOA which will allow for the mounting of a QO breaker such as a QO240 .


CTA-ID : 2050887
Was this helpful?
What can we do to improve the information ?