Technical FAQs

Ask a Question

Can you order the receiver only or a transmitter only for a XUSLPZ3A0500M? <br />

Yes,
To order a receiver only, add the letter R to the end of the reference number of the Transmitter-Receiver pair, making the part number a XUSLPZ3A0500MR.

To order a transmitter only, add the letter T to the end of the reference number of the Transmitter-Receiver pair, making the part number a XUSLPZ3A0500MT.


CTA-ID : 2050886
Was this helpful?
What can we do to improve the information ?