Technical FAQs

Ask a Question

Will a two pole GFI breaker work if you do not connect the pigtail?

Yes, the GFI module will operate if there is between 100V and 140V between any two poles. The push-to-test will not work if the pigtail is not connected.

CTA-ID : 2051663
Was this helpful?
What can we do to improve the information ?