Technical FAQs

Ask a Question

What is the size of the transition section for 5/15kV NEMA 3R outdoor HVL/cc to MasterClad metalclad switchgear?

Issue:
What is the size of the transition section for 5/15kV NEMA 3R outdoor HVL/cc to MasterClad metalclad switchgear?

Product Line:
MasterClad.

Environment:
Products sold in the United states.

Cause:
Product features.

Resolution:
The section is 22" wide plus a 3" collar. Approximately 60" deep and 90" high. This is for rear alignment.


CTA-ID : 2051465
Was this helpful?
What can we do to improve the information ?