Technical FAQs

Ask a Question

Is the HVL standard NEMA 3R roof one piece? Is it welded?

Issue:
Is the HVL standard NEMA 3R roof one piece? Is it welded?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, the standard HVL roof for outdoor NEMA 3R is one piece.

It is not welded. The roof has flanges on the sides which turn up and then are covered by roof rabbets.


CTA-ID : 2051445
Was this helpful?
What can we do to improve the information ?