Technical FAQs

Ask a Question

Can a QONQ42MS400 load center be either top or bottom fed?

Product Design features

Product Line:
QO load centers

Service conductor feed

Application/ insallation

The interior is set up for bottom feed as standard. For a top feed application, first rotate the main breaker 180 degrees, then rotate the entire load center interior 180 degrees.
NOTE: When the interior is rotated, the deadfront trim labels will be upside down. 

CTA-ID : 2050877
Was this helpful?
What can we do to improve the information ?