Technical FAQs

Ask a Question

Is there a guard that will work with the 2 1/4 inch mushroom operator on a push pull operator, 9001KR8, 9001KR9?<br /><br />

No. There isn`t a guard available for the ``push pull`` operator with a 2 1/4 inch mushroom knob that has finger cut outs to pull the operator back out.

CTA-ID : 2051451
Was this helpful?
What can we do to improve the information ?