Technical FAQs

Ask a Question

What is the metal mounting stand for a 9036GG2R?<br /><br />REVISION R#2010006 (Correct catalog number 9049UBS1 to 9049UMS1)

A 9049UMS1 is a 3/16`` metal plate with thread hole in center for a customer suplied 1`` black pipe of the desired length. It attaches to the bottom of all 9035, all 9036, 9038AG, AR & AW float switches.

CTA-ID : 2051579
Was this helpful?
What can we do to improve the information ?