Technical FAQs

Ask a Question

What type of fuse do the DF101 and DF101V holders accept?

The fuseholders accept aM cartridge fuses refer to Catalog 9080CT0801page 6.
The fuse size is mm 10 x 38 and (Inch) (0.4 x 1.5).

CTA-ID : 2051907
Was this helpful?
What can we do to improve the information ?