Technical FAQs

Ask a Question

Can you use compression lugs on a EZM11600CB or a EZM31600CB?

You can install up to 6 compression lugs per phase and neutral. Examples: Anderson VHCL60012BN which is good for 250 MCM to 600 MCM copper, or VHCL75012BN which is good for 500MCM to 750MCM copper.


CTA-ID : 2051639
Was this helpful?
What can we do to improve the information ?