Technical FAQs

Ask a Question

Where did one select the Intelligent Load Center catalog numbers from?

Issue:
Product Design Features

Product Line:
QO Load Centers 

Environment:
Automatic transfer Switch and control panel

Cause:
Application

Resolution
NOTE: ALL the ILC(Intelligent Load Center) catalog numbers have been obsoleted and are NO longer available with NO replacements.

When the ILC catalog numbers were available, they were found in the lastest version of the Digest or the On-Line Digest.
Also, the owner would go to www.kohlerpowersystems.com and should be able to see a list of all their distributors. The Kohler Distributor can give them a list of the dealers in that area. If not, they can call Kohler at 800-544-2444 and ask for this information.

 
Was this helpful?
What can we do to improve the information ?